This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIEVM-HV-1PH-DCAC: Inverter Digital Control Loop / Consultant Referral

Part Number: TIEVM-HV-1PH-DCAC


Hi There,

We ae using the TIEVM-HV-1PH-DCAC Single Phase Inverter Reference Design on a project where we are adapting this design to generate inverter output at frequencies from 50 Hz up to 800 Hz and have not been able to adjust control system parameters to produce a stable output when making required adjustments to the H-Bridge output filter to support the higher frequency range.  Do you know of a consultant or consultancy group that would have the expertise to support an effort to tune the C2000 control loop algorithm and parameters for this configuration? 

Appreciate any help here. 

Mike