Part Number: TMS320F28075
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I try to use the example code for CAN communication
C:\ti\controlSUITE\device_support\F2807x\v180\F2807x_examples_Cpu1\can_loopback_interrupts
I face 2 problems
1.
I keep it in external loopback mode and change its GPIO pins, but change GPIO31-CANTXA to something other than GPIO31, such as GPIO_SetupPinMux (32, GPIO_MUX_CPU1, 1), an error will occur, and I find the point where the error occurred is ulStatus & ~ (CAN_ES_TXOK | CAN_ES_RXOK)) == 5, what is the problem with this?
2.
I removed the external loopback mode and changed it to CAN communication. Annotate HWREG (CANA_BASE + CAN_O_CTL) | = CAN_CTL_TEST; HWREG (CANA_BASE + CAN_O_TEST) = CAN_TEST_EXL;
Change the GPIO setting to GPIO_SetupPinMux (70, GPIO_MUX_CPU1, 6);
// GPIO31-CANTXA
GPIO_SetupPinMux (71, GPIO_MUX_CPU1, 6);
GPIO_SetupPinOptions (70, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinOptions (71, GPIO_OUTPUT, GPIO_PUSHPULL);
I can send messages, but I still ca n’t receive them. Is there something I missed?
The complete code is as follows:
//###########################################################################
// FILE: can_loopback_interrupts.c
// TITLE: Example to demonstrate basic CAN setup and use.
//
//! \addtogroup cpu01_example_list
//! <h1>CAN External Loopback with Interrupts (can_loopback_interrupts)</h1>
//!
//! This example shows the basic setup of CAN in order to transmit and receive
//! messages on the CAN bus. The CAN peripheral is configured to transmit
//! messages with a specific CAN ID. A message is then transmitted once per
//! second, using a simple delay loop for timing. The message that is sent is
//! a 4 byte message that contains an incrementing pattern. A CAN interrupt
//! handler is used to confirm message transmission and count the number of
//! messages that have been sent.
//!
//! This example sets up the CAN controller in External Loopback test mode.
//! Data transmitted is visible on the CAN0TX pin and can be received with
//! an appropriate mailbox configuration.
//!
//! This example uses the following interrupt handlers:\n
//! - INT_CANA0 - CANIntHandler
//!
//
//###########################################################################
// $TI Release: F2807x Support Library v180 $
// $Release Date: Fri Nov 6 16:33:02 CST 2015 $
// $Copyright: Copyright (C) 2014-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#include "F28x_Project.h" // Device Headerfile and Examples Include File
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_can.h"
#include "driverlib/can.h"
//*****************************************************************************
// A counter that keeps track of the number of times the TX interrupt has
// occurred, which should match the number of TX messages that were sent.
//*****************************************************************************
volatile unsigned long g_ulTxMsgCount = 0;
volatile unsigned long g_ulRxMsgCount = 0;
int i;
//unsigned long u32CanAErrorStatus;
//unsigned long uCanAErrFlag;
//*****************************************************************************
// A flag to indicate that some transmission error occurred.
//*****************************************************************************
volatile unsigned long g_bErrFlag = 0;
tCANMsgObject sTXCANMessage;
tCANMsgObject sRXCANMessage;
unsigned char ucTXMsgData[8] ={ 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };
unsigned char ucRXMsgData[8];
//unsigned long u32CntTXMsgData = 0x12345678;
//*****************************************************************************
// This function is the interrupt handler for the CAN peripheral. It checks
// for the cause of the interrupt, and maintains a count of all messages that
// have been transmitted.
//*****************************************************************************
interrupt void
CANIntHandler(void)
{
unsigned long ulStatus;
// Read the CAN interrupt status to find the cause of the interrupt
ulStatus = CANIntStatus(CANA_BASE, CAN_INT_STS_CAUSE);
// If the cause is a controller status interrupt, then get the status
if(ulStatus == CAN_INT_INT0ID_STATUS)
{
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Error processing
// is not done in this example for simplicity. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt. If the
// CAN peripheral is not connected to a CAN bus with other CAN devices
// present, then errors will occur and will be indicated in the
// controller status.
ulStatus = CANStatusGet(CANA_BASE, CAN_STS_CONTROL);
//Check to see if an error occurred.
if(((ulStatus & ~(CAN_ES_TXOK | CAN_ES_RXOK)) != 7) &&
((ulStatus & ~(CAN_ES_TXOK | CAN_ES_RXOK)) != 0)){
// Set a flag to indicate some errors may have occurred.
g_bErrFlag = 1;
}
}
// Check if the cause is message object 1, which what we are using for
// sending messages.
else if(ulStatus == 1)
{
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
CANIntClear(CANA_BASE, 1);
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
g_ulTxMsgCount++;
// Since the message was sent, clear any error flags.
g_bErrFlag = 0;
}
// Check if the cause is message object 1, which what we are using for
// receiving messages.
else if(ulStatus == 2)
{
// Get the received message
CANMessageGet(CANA_BASE, 2, &sRXCANMessage, true);
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
CANIntClear(CANA_BASE, 2);
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
g_ulRxMsgCount++;
// Since the message was sent, clear any error flags.
g_bErrFlag = 0;
}
// Otherwise, something unexpected caused the interrupt. This should
// never happen.
else
{
// Spurious interrupt handling can go here.
}
//canaRegs.CAN_GLB_INT_CLR.bit.INT0_FLG_CLR = 1;
CANGlobalIntClear(CANA_BASE, CAN_GLB_INT_CANINT0);
PieCtrlRegs.PIEACK.all = PIEACK_GROUP9;
}
//*****************************************************************************
// Configure the CAN and enter a loop to transmit periodic CAN messages.
//*****************************************************************************
int main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2807x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initialize GPIO:
// This example function is found in the F2807x_Gpio.c file and
// illustrates how to set the GPIO to its default state.
InitGpio();
//GPIO 73 - XCLKOUT
//GPIO_SetupPinMux(73, GPIO_MUX_CPU1, 3);
//GPIO_SetupPinOptions(73, GPIO_OUTPUT, GPIO_PUSHPULL); // -> SYSCLOCK/8 = 25MHz
//GpioCtrlRegs.GPAMUX1.bit.GPIO10=0;
//GpioCtrlRegs.GPADIR.bit.GPIO10=0;
//GpioDataRegs.GPADAT.bit.GPIO10=0;
//GPIO30 - CANRXA
GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 6);
//GPIO31 - CANTXA
GPIO_SetupPinMux(71, GPIO_MUX_CPU1, 6);
GPIO_SetupPinOptions(70, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinOptions(71, GPIO_OUTPUT, GPIO_PUSHPULL);
//GPIO30 - CANRXB
//GPIO_SetupPinMux(73, GPIO_MUX_CPU1, 6);
//GPIO31 - CANTXB
//GPIO_SetupPinMux(72, GPIO_MUX_CPU1, 6);
//GPIO_SetupPinOptions(73, GPIO_INPUT, GPIO_ASYNC);
//GPIO_SetupPinOptions(72, GPIO_OUTPUT, GPIO_PUSHPULL);
// Initialize the CAN controller
CANInit(CANA_BASE);
//CANInit(CANB_BASE);
// Setup CAN to be clocked off the PLL output clock
CANClkSourceSelect(CANA_BASE, 0); /* 500kHz CAN-Clock */
// Set up the bit rate for the CAN bus. This function sets up the CAN
// bus timing for a nominal configuration. You can achieve more control
// over the CAN bus timing by using the function CANBitTimingSet() instead
// of this one, if needed.
// In this example, the CAN bus is set to 500 kHz. In the function below,
// the call to SysCtlClockGet() is used to determine the clock rate that
// is used for clocking the CAN peripheral. This can be replaced with a
// fixed value if you know the value of the system clock, saving the extra
// function call. For some parts, the CAN peripheral is clocked by a fixed
// 8 MHz regardless of the system clock in which case the call to
// SysCtlClockGet() should be replaced with 8000000. Consult the data
// sheet for more information about CAN peripheral clocking.
CANBitRateSet(CANA_BASE, 120000000, 500000);
//CANBitRateSet(CANA_BASE, 120000000, 1000000);
// Enable interrupts on the CAN peripheral. This example uses static
// allocation of interrupt handlers which means the name of the handler
// is in the vector table of startup code. If you want to use dynamic
// allocation of the vector table, then you must also call CANIntRegister()
// here.
//CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2807x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2807x_DefaultIsr.c.
// This function is found in F2807x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
// Register interrupt handler in RAM vector table
EALLOW;
PieVectTable.CANA0_INT = CANIntHandler;
EDIS;
// Enable the CAN interrupt on the processor (PIE).
PieCtrlRegs.PIEIER9.bit.INTx5 = 1;
IER |= 0x0100; /* M_INT9 */
EINT;
// Enable test mode and select external loopback
//HWREG(CANA_BASE + CAN_O_CTL) |= CAN_CTL_TEST;
//HWREG(CANA_BASE + CAN_O_TEST) = CAN_TEST_EXL;
// Enable the CAN for operation.
CANEnable(CANA_BASE);
//CANEnable(CANB_BASE);
CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0);
// Initialize the message object that will be used for sending CAN
// messages. The message will be 4 bytes that will contain an incrementing
// value. Initially it will be set to 0x12345678.
//ucTXMsgData[0] = (u32CntTXMsgData>>24) & 0xFF;
//ucTXMsgData[1] = (u32CntTXMsgData>>16) & 0xFF;
//ucTXMsgData[2] = (u32CntTXMsgData>>8) & 0xFF;
//ucTXMsgData[3] = (u32CntTXMsgData) & 0xFF;
sTXCANMessage.ui32MsgID = 1; // CAN message ID - use 1
sTXCANMessage.ui32MsgIDMask = 0; // no mask needed for TX
sTXCANMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE; // enable interrupt on TX
sTXCANMessage.ui32MsgLen = sizeof(ucTXMsgData); // size of message is 8
sTXCANMessage.pucMsgData = ucTXMsgData; // ptr to message content
// Initialize the message object that will be used for receiving CAN
// messages.
*(unsigned long *)ucRXMsgData = 0;
sRXCANMessage.ui32MsgID = 1; // CAN message ID - use 1
sRXCANMessage.ui32MsgIDMask = 0; // no mask needed for TX
sRXCANMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE; //MSG_OBJ_USE_EXT_FILTER | MSG_OBJ_EXTENDED_ID; // enable interrupt on RX
sRXCANMessage.ui32MsgLen = sizeof(ucRXMsgData); // size of message is 8
sRXCANMessage.pucMsgData = ucRXMsgData; // ptr to message content
// Setup the message object being used to receive messages
CANMessageSet(CANA_BASE, 2, &sRXCANMessage, MSG_OBJ_TYPE_RX);
// Send the CAN message using object number 1 (not the same thing as
// CAN ID, which is also 1 in this example). This function will cause
// the message to be transmitted right away.
ucTXMsgData[0] = 0x12;
ucTXMsgData[1] = 0x34;
ucTXMsgData[2] = 0x56;
ucTXMsgData[3] = 0x78;
// Enter loop to send messages. A new message will be sent once per
// second. The 4 bytes of message content will be treated as an unsigned
// long and incremented by one each time.
for(;;)
{
// Check the error flag to see if errors occurred
if(g_bErrFlag)
{
asm(" ESTOP0");
}
if(g_ulTxMsgCount == g_ulRxMsgCount){
CANMessageSet(CANA_BASE, 1, &sTXCANMessage, MSG_OBJ_TYPE_TX);
}else{
//g_bErrFlag = 1;
}
// Now wait 1 second before continuing
DELAY_US(1000*1000);
// Increment the value in the transmitted message data.
ucTXMsgData[0]+= 0x01;
ucTXMsgData[1]+= 0x01;
ucTXMsgData[2]+= 0x01;
ucTXMsgData[3]+= 0x01;
}
}