This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069M: CCS/LAUNCHXL-F28069M: Code do not start when using external power

Part Number: TMS320F28069M
Other Parts Discussed in Thread: LAUNCHXL-F28069M

Tool/software: Code Composer Studio

Hello!
I was doing some tests, and I noticed a little problem with the LAUNCHXL-F28069M development board.
Whenever I feed it externally (not via USB) the processor does not start, I need to plug in the USB for the code to run. Also, if I turn off the external power, even with the USB connected, the code does not start, I need to unplug and plug the USB again to start the execution. I tested this with several codes including the launchpad example, and the same effect occurs. How do I fix this?
Thanks.