This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: SYS/BIOS .cfg graphical user interface XGCONF

Expert 1190 points
Part Number: TMS320F28377S

Tool/software: Code Composer Studio

hello. the graphical user interface does not appear  when double clicking on the XGCONFG this is not the case when Sample Projects are imported.

Created with CC9

Sample Project:

Added .XFG

sample projects  have a sys/bios appended

Projects with .cfg added,  (add cfg : New->XXX->RTSC XXXX.cfg)

Is a  demo sys/bios  blink project available ?

thanks

  • How does one add cut and paste to thread, with firefox

  • For attaching images there is a button on the toolbar just above the text box.  It allows you to point to an image file that will then be uploaded and inserted into the thread. 

    By default CCS uses a text editor for .cfg files.  You can still use the graphical editor by right clicking on the file in Project Explorer and selecting to use XGCONF.

    After you do that once it will use it as the new default editor.

    Regards,

    John