Other Parts Discussed in Thread: C2000WARE
I am testing an implementation for the HRPWM on the TMS28379D DSP.
I have modified an example provided in control suite.
For ease of use, I changed the UPDOWN count to UP count in the PWM init of the example.
Dear C2000 team,
the behavior I am seeing when I set the PWM parameters to 500 kHz and 0.5 DC is correct.
When I change to 501 kHz and the HR part of the PWM is used, on my scope I can only measure a jittered PWM between 500 kHz and 502.5 kHz. This is also available for any value in the TBPRDHR register.
The TBPRD and TBPRDHR registers seem to update correctly.
Is this the intended behavior? If so how would I go about measuring the precision of the system?
If not, I have attached the c file I modified, maybe I missed something?
Please let me know