Hi
In my CPU design, pin XRS is left unconnected. (80 pin package, pin number 9)
I do not use this pin to assert input external RESET by HW.
I do not use the watchdog reset output either.
My question is: May I leave this pin not connected, or should I follow the statement in Datasheet (page 15) which states to place a Pull-Up resistor (and a possible cap)?
If pull up is required, then I must re-layout my board, or add quite a complicated "stitch" , manually , by soldering an appropriate resistor on the PCB.