Part Number: TMS320F28334
Tool/software: Code Composer Studio
Hello,
I need to receive more than 32 CAN-IDs, so I have trying to assign multiple CAN-IDs to one mailbox.
CAN-ID are 0xDFFFF100 and 0x1DFFFF101 (omitted for simplicity, described only 2 ID).
Initialized as below;
EcanaLAMRegs.LAM0.all = 0;
EcanaLAMRegs.LAM0.bit.LAMI = 1;
EcanaLAMRegs.LAM0.bit.LAM_L = 0xf;
EcanaMboxes.MBOX0.MSGID.all = 0xDFFFF100;
EcanaLAMRegs.LAM1.all = 0;
EcanaLAMRegs.LAM1.bit.LAMI = 1;
EcanaLAMRegs.LAM1.bit.LAM_L = 0xf;
EcanaMboxes.MBOX1.MSGID.all = 0xDFFFF100;
Then, I receive as below:
receive_bits = ECanaRegs.CANRMP.all & CAN_RECV_MASK;
EcanaRegs.CANRMP.all = receive_bits;
if ((receive_bits & BIT0) != 0) {
// Analyze data (1)
}
if ((receive_bits & BIT1) != 0 ) {
// Analyze data (2)
}
I want to put 0xDFFFF100 and 0xDFFFF101 in each MBOX but not set to Analyze data (1), set only Analyze data (2) whatever 0xDFFFF100 or 0xDFFFF101.
What are the missing setting?
Thank you,