Part Number: TMS320F28388D
Greetings,
Am running the FCL project using the 28388 card plugged in to the Industrial drive experimenters board.
I have a 3phase BLDC motor with incremental encoder. I am able to run the project at level 2. The motor spins when the VqTesting level is set to 0.2 or above. 0.2 give the smoothest motion. The motor runs open loop fine and the speedRef value allows chaning the RPM.
When I switch to level 3 , the motor does not spin and only vibrates.
Not sure what I am missing here, any poke in the right direction will be appreciated.
David