Part Number: TMS320F28377D
Tool/software: Code Composer Studio
Hi:
I am trying to get access to addresses from 0x00100000 to 0x00100008, which in the CS2 area. Follow the Technical Reference Manual, EMIF has been configured as the asynchronous mode. For reading/writing 16-bit words, A0 is connected to EMxBA1, [A7: A1] are connected to [A6: A0]. However, form the logical analyzer (Signaltap II), 28377d is not output correct address. CS2 signal kept at 1. RNW at 0. AWE at 1. In addition, the pointer monitored in CCS is correct. It is quite strange.
I attached my code. Could somebody give me a hint? Many Thanks.
#include "F28x_Project.h"
void main(void)
{
InitSysCtrl();
EALLOW;
ClkCfgRegs.PERCLKDIVSEL.bit.EMIF1CLKDIV = 1; // PLLSYSCLK 1/2 for EMIF
EDIS;
InitGpio();
EALLOW;
//led
GpioCtrlRegs.GPEMUX1.bit.GPIO133=0;
GpioCtrlRegs.GPEDIR.bit.GPIO133=1;
//cs2 rd we
GpioCtrlRegs.GPBMUX1.bit.GPIO32=2; //cs0 LOW ENABLE
GpioCtrlRegs.GPBMUX1.bit.GPIO34=2; //cs2 LOW ENABLE
GpioCtrlRegs.GPBMUX1.bit.GPIO33=2; //RNW HIGH ENABLE
GpioCtrlRegs.GPAMUX2.bit.GPIO31=2; //WE LOW ENABLE
GpioCtrlRegs.GPBMUX1.bit.GPIO37=2; //EM1OE LOW ENABLE
//addr
GpioCtrlRegs.GPCMUX2.bit.GPIO92=3; //EM1BA1
GpioCtrlRegs.GPBMUX1.bit.GPIO38=2; //A0
GpioCtrlRegs.GPBMUX1.bit.GPIO39=2; //A1
GpioCtrlRegs.GPBMUX1.bit.GPIO40=2; //A2
GpioCtrlRegs.GPBMUX1.bit.GPIO41=2; //A3
GpioCtrlRegs.GPBMUX1.bit.GPIO44=2; //A4
GpioCtrlRegs.GPBMUX1.bit.GPIO45=2; //A5
GpioCtrlRegs.GPBMUX1.bit.GPIO46=2; //A6
GpioCtrlRegs.GPBMUX1.bit.GPIO47=2; //A7
GpioCtrlRegs.GPBMUX2.bit.GPIO48=2; //A8
GpioCtrlRegs.GPBMUX2.bit.GPIO49=2; //A9
GpioCtrlRegs.GPBMUX2.bit.GPIO50=2; //A10
GpioCtrlRegs.GPBMUX2.bit.GPIO51=2; //A11
GpioCtrlRegs.GPBMUX2.bit.GPIO52=2; //A12
GpioCtrlRegs.GPCMUX2.bit.GPIO86=2; //A13
GpioCtrlRegs.GPCMUX2.bit.GPIO87=2; //A14
GpioCtrlRegs.GPCMUX2.bit.GPIO88=2; //A15
GpioCtrlRegs.GPCMUX2.bit.GPIO89=2; //A16
GpioCtrlRegs.GPCMUX2.bit.GPIO90=2; //A17
GpioCtrlRegs.GPCMUX2.bit.GPIO91=2; //A18
//GpioCtrlRegs.GPCMUX2.bit.GPIO92=2; //A19
//data
GpioCtrlRegs.GPCMUX1.bit.GPIO69=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO70=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO71=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO72=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO73=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO74=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO75=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO76=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO77=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO78=2;
GpioCtrlRegs.GPCMUX1.bit.GPIO79=2;
GpioCtrlRegs.GPCMUX2.bit.GPIO80=2;
GpioCtrlRegs.GPCMUX2.bit.GPIO81=2;
GpioCtrlRegs.GPCMUX2.bit.GPIO82=2;
GpioCtrlRegs.GPCMUX2.bit.GPIO83=2;
GpioCtrlRegs.GPCMUX2.bit.GPIO85=2;
EDIS;
Emif1Regs.ASYNC_CS2_CR.all = (EMIF_ASYNC_ASIZE_16 | //16位内存
EMIF_ASYNC_TA_4 |
EMIF_ASYNC_RHOLD_8 |
EMIF_ASYNC_RSTROBE_64 |
EMIF_ASYNC_RSETUP_16 |
EMIF_ASYNC_WHOLD_8 |
EMIF_ASYNC_WSTROBE_64 |
EMIF_ASYNC_WSETUP_16 |
EMIF_ASYNC_EW_DISABLE |
EMIF_ASYNC_SS_DISABLE);
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EINT;
int i;
Uint16 *ExRamStart = (Uint16*)0x00100000;
for(i=0; i<0x0008; i++)
{
*(ExRamStart+i)=0x6666;
}
while(1)
{
GpioDataRegs.GPECLEAR.bit.GPIO133=1;
DELAY_US (500000);
GpioDataRegs.GPESET.bit.GPIO133=1;
DELAY_US (500000);
}
}