Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8301, MOTORWARE, CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
I liked the fact InstaSPIN™ BLDC Lab do, and I would like to run this lab, however the current hardware I have in hand, is F28069M launchpad, DRV8301 Boosterpack, & a 12 V power supply, and the motor ofcourse.
Is it possible to run this lab with these hardwares ? If yes, are there any additional changes (other than Jumpers) that I should modify on the launchpad?
Thanks.