Part Number: BOOSTXL-DRV8301
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Hi again :) ,
Reading about InstaSPIN-FOC on TI website it says,
Motor identification
- No datasheet required
- One time parameter identification based on simple motor nameplate data (max voltage, current)
But in instaspin_labs guide only these values should be identified
|
USER_MOTOR_MAX_CURRENT |
where should we modify the max voltage ?
And should we have power supply to the motor the same as the nameplate (max) Voltage ? As the Current may deviate from the nameplate amperes if the voltage turns out to be lower than indicated. I'm a bit confused with these two points.
One more thing Why are there additional modifications only stated in qsg_gui_universal ? slide 25/55 (//! \brief CURRENTS AND VOLTAGES )
Thanks