HELLO:
Is it possible to take the basic design & use three of these - drive each to get 0, 120 & 240 phase-shifted sinusoidal output power thus making a modern digitally controlled 3 phase lab-grade power source of 2400VA?
Question is really: how to make the output sinusoids to have 3 phases from the controller PWMs
Would it work in the lab if we got three eval kits & modified the code to cause the phase shifts at each of the outputs?
What will cause them to be synchronous
-robin