This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/F28M36P63C2: Examples to implement default gateway using F28m36 concerto device

Part Number: F28M36P63C2

Tool/software: Code Composer Studio

Hello all,

I am having trouble with one of my projects. I have been using the enet_uip.c file on control suite to implement Ethernet remote access to a power converter unit. it's a simple application that creates a web page that can be used to monitor fault status and engage several GPIO's on the f28m36 board embedded in the power converter. As of now the application uses a static IP address

I want to add a default gateway to the firmware so that the device is able to do network translation and be capable of transmitting traffic to other devices on the network. Are there any examples or documentation on how to implement this for the concerto device. Any help or suggestion is greatly appreciated.

Thanks for your time

Srini