Is the interrupt latency variable on the 28035?
I'm running PWM3 (at 50 kHz) with an interrupt on time compare at 2 us. The first instruction on the ISR toggles GPIO6. I expected to be a bit of a delay between the 2 us time and the toggle of GPIO6 (as seen on a scope). My question is if this is supposed to be variable (about 400 ns between the smallest and the largest). There is no other interrupt.