This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSPREX28335: Connect android app with TMDSPREX28335

Part Number: TMDSPREX28335
Other Parts Discussed in Thread: C2000WARE

Hi all,

I want to connect an android app with TMDSPREX28335. The android app will take user inputs and send to TMDSPREX28335 board for giving input to a pre running control algorithm dumped using MATLAB/Simulink. The android app will also display data sent from TMDSPREX28335 borad in the display board.

I have searched a lot for implementing the idea but could not find any soultion. Can anyone share any experience of doing so or suggest the way to do it.

Bikash

  • Bikash,

    You could consider communicating with the Peripheral Explorer Kit using the SCI/UART.  One method is to use the USB connection, and jumper J4 would need to be populated (see the schematic in C2000Ware for details).  Another method is to use the SCI/UART header pins.

    As an additional resource for SCI/UART communications with the Peripheral Explorer Kit (but it is very old) please see module 9 under the C2833x_CCS4 folder in the C2000 Teaching ROM:

    http://www.ti.com/lit/zip/ssqc019

     I hope this helps. If this answers your question, please click the green "Verified Answer" button. Thanks.

    - Ken

  • Bikash,

    It's been a while since I have heard from you last. Therefore, I am assuming you were able to resolve your issue and I will close this thread. If this isn’t the case, please reject this resolution or reply to this thread. If this thread locks, please make a new thread describing the current status of your issue. Thank you.

    - Ken