Unable to perform External mode operation over Serial Communication for Signal monitoring in Simulink using Embedded Coder Support Package. The following configuration parameters have been already done ( screenshots of which are attached herewith). The simulink model although can be built successfully but the Serial communication interface cannot be established with TMS320F28069 control card with a error message. (Also shown in screenshot).