Other Parts Discussed in Thread: SPRC141
I am programing a motor drive board with a TMS320LF2407APAGA. I haveing a problem with Flash. I am using CCS3.3. For a test I am trying to program c_coxist from SPRC141. It builds ok, but when I use the ON-Chip Flash Programmer (CCS3.3) I get:
**** Begin Sector Clear Operation ****
OK: Flash Algorithm loaded into DSP memory
OK: Write sector value 0x000f to symbol PRG_options
OK: Set Breakpoint at PRG_stop
OK: Running flash algorithm
OK: DSP Halted
OK: Read status value 0x0000 from symbol PRG_status
OK: PC set to PRG_erase
OK: Running flash algorithm
OK: DSP Halted
Error: Read status value 0x0001 from symbol PRG_status
Flash algorithm failed during clear operation
The Code Security Password keeps changing, I have to VIEW Memory (0x4) for the new password. Thus over writing my cmd file from SPRC141 is :
/*--------------------------------------------------------------------------------------------------
* Filename : MAIN.CMD
* Last Modified : 26 Dec 2001.
* Version : 1.3
* Originator : Texas Instruments, DSP Digital Control Systems Group.
*--------------------------------------------------------------------------------------------------
* Revision history :
*
* Version 1.3 (2 Jan 2002):
* * Added header which was missing.
* * Added allocation for .bss and .stack sections.
* * Modified memory block PROG to start at 0x44, so as to
* keep out of the password area on the rev-A parts
*
*/
MEMORY
{
PAGE 0 : VECS: origin = 0x0000, length = 0x0040
PAGE 0 : PROG: origin = 0x0000, length = 0x7fbc
PAGE 0 : ABSRAM: origin = 0x8000, length = 0x0040
PAGE 0 : SARAM: origin = 0x8040, length = 0x07c0
PAGE 1 : BLKB2: origin = 0x0060, length = 0x0020
PAGE 1 : BLKB0B1: origin = 0x0200, length = 0x02ff
}
SECTIONS
{
VECTORS : {} > VECS PAGE 0
.text : {} > PROG PAGE 0
.cinit : {} > PROG PAGE 0
/* Allocate the relocation sensitive portions in SARAM
at proper addresses. The relocation sensitive section
should always be sent to a RAM block starting on XXX0
for the relocation mechanism to properly locate the
code with relocation sensitivities.
*/
UNION run = ABSRAM PAGE 0
{
CSPL_tex: load = PROG PAGE 0
{
.+= 7;
ClearAlgoRunSpl = . ;
*(CSPL_text)
}
PSPL_tex: load = PROG PAGE 0
{
.+= 7;
ProgramAlgoRunSpl = . ;
*(PSPL_text)
}
ESPL_tex: load = PROG PAGE 0
{
.+= 7;
EraseAlgoRunSpl = . ;
*(ESPL_text)
}
}
UNION run = SARAM PAGE 0
{
CLR_text: load = PROG PAGE 0
{
ClearAlgoRunMain = . ;
}
ERA_text: load = PROG PAGE 0
{
EraseAlgoRunMain = . ;
}
PGM_text load = PROG PAGE 0
{
ProgramAlgoRunMain = . ;
}
}
KER_comp : load = PROG PAGE 0, run = SARAM PAGE 0
{
KernelRun = .;
*(KER_strt)
*(KER_text)
*(KER_end)
}
.flshvar : {} > BLKB2 PAGE 1
.bss : {} > BLKB0B1 PAGE 1
.stack : {} > BLKB0B1 PAGE 1
}
I am fimiliar w/ flashing 2812, I am not sure what I am missing for the Lf2407
Thank
John