This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F2812: Migrating to CCS6.2 from CCS5.5, Getting error in compilation

Part Number: TMS320F2812
Other Parts Discussed in Thread: SYSBIOS, C2000WARE

Tool/software: Code Composer Studio

Dear All, 

Greetings. I am getting an error during compilation that says "XDAIS v0.0 is not currently installed and no compatible version is available. Please install this product"

Earlier the project was compiled using CCS5.5 However we had to migrate to CCS6.2 due to windows compatibility reasons. After installing CCS6.2 we are getting the above error. 

Can any one shed any light on this error.. I have tried uninstalling and then reinstalling CCS6.2 But it has not helped so far. 

ANY help would be highly appreciated.

Best Regards

Anand