Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am developing a Bootloader on a Canbus for the F28379D.
I already have a PCB where CanA uses pins 30 and 31, is it possible to have the source code for the boot rom, so I can adapt it and include it in my code?
I only need the can part.
Also, I was reading the reference manual and I found a reference to two "test mode" can boot loaders, what are they?
0x47 CANBOOT(TEST)(0) ± TESTMODE
0xC7 CANBOOT(TEST)(1) ± TEESTMODE, Alternate
(Pag 612 of document spruhm8i.pdf)
Can they be useful to debug something?
PS
here https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/598593?LAUNCHXL-F28379D-LaunchPad-will-support-to-boot-from-CAN-Please-clarify Harshmeet stated that CanBoot mode can use pins 36 and 37;
however from http://www.ti.com/lit/ds/symlink/tms320f28379d.pdf, pag 198, there is this
CAN-Boot0 CANRXA: GPIO70 CANTXA: GPIO71 CAN-A Boot – I/O option 1
CAN-Boot1 CANRXA: GPIO62 CANTXA: GPIO63 CAN-A Boot – I/O option 2
You might want to add a note on that forum that there was a mistake in the second pin option.