Hi,
I am planning on using the TMS320F28388D ADC in 16-bit differential input mode with a Vref of 2.5V. I notice with other ADCs sometimes I see that there are mini low pass RC filter in between the buffer and the ADC input. From the specification, I am assuming that I want to keep the Rs and Cp to a minimimum to maximize settling time. Does TI recommend just connecting the output of the differential buffer directly to the ADC input or should I put an option to populate an RC filter?
Thanks,
Jennifer