Other Parts Discussed in Thread: TL431
Hello
I have problem with ADC again unfortunately. I use ezdsp f28335 for controlling dc dc boost converter and three phase inverter. At first ,if anyone has used this kit before, what is the the input range of ADC? Is it 3 V like 2812 or 1,9 V?
I use MAtlab Simulink to program DSP. When I change ADC input to 1 V, ePWM duty cycle changes but after the input of ADC is bigger than 1 V it begins to draw 30, 40, 50 mA and more (I tried to 70 mA).Is it normal? I have no other dsp to try.
The other question how can I protect the ADC? I designed a voltage sensing circuit. There is a zener diode, a serial resistor to limit the current, there are protection diodes (not to pass 2.7 V and not to go negative) . I send the schematic circuit below? In spite of these protection can the ADC modules be damaged. AS I said it makes normal control to 1 V.
I am very confused again. Thanks from now...