This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bootloading c2000prog uart using other controller

hi every1,

i have two controllers, one of them is 2812 controller, and i want to make bootload through the other controller,

now i can successfully program the DSP using the C2000prog (CodeSkin), and the HEX file, 

what shall i do to make the controller do exactly like the C2000prog.

i have compared the HEX file generated with the HEX file has been sent by C2000prog, but they are not the same,,,,

again the problem:

1- i can send HEX file through the other controller but which HEX file will work,,,

 

regards