This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ezdsp f28335 target configuration file

Hi, I trying to connect the ezdsp f28335 starter kit to CCS V4. What should be selected from the 'Connection'  and the 'Board and Device' drop down menus to successfully create the right target configuration file which can be used with the example projects. My board is connected to the computer via a USB and whenever I try debugging, I'm unable to connect to connect to the target device. 

  • Shoaib Hussain said:

    Hi, I trying to connect the ezdsp f28335 starter kit to CCS V4. What should be selected from the 'Connection'  and the 'Board and Device' drop down menus to successfully create the right target configuration file which can be used with the example projects. My board is connected to the computer via a USB and whenever I try debugging, I'm unable to connect to connect to the target device. 

    Shoaib,

    I believe it is the "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" for the connection.  And then EZDSPF28335 for the Device.

    -Lori