Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi all,
I am using the TMS320F28379D launchpad. I used the device.h to include pin definition.
I have a compilation problem when I include the device.h header file,
"C:/ti/c2000/C2000Ware_2_00_00_03/driverlib/f2837xd/driverlib/adc.h", line 176: error #41: expected an identifier
"C:/ti/c2000/C2000Ware_2_00_00_03/driverlib/f2837xd/driverlib/adc.h", line 177: error #41: expected an identifier
In the adc.h file, the compiler prompted "expected an identifier" to the following lines
typedef enum
{
ADC_RESOLUTION_12BIT = 0x00, //!< 12-bit conversion resolution
ADC_RESOLUTION_16BIT = 0x40 //!< 16-bit conversion resolution
} ADC_Resolution;
S.Tarik,