Part Number: TMS320F280049C
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
i got the launchpad, had already installed the CCC, but the debugger does not start. comes up with this error:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 9.1.0.00001)
i tried to re-install the drivers from here, but no change:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/emulation/exports/ti_emupack_setup_9.1.0.00001_win_64.exe?tracked=1
help