Hello,
I have a very simple application where I want to use the F28335's epwm module to generate a tone for a piezo buzzer.
Here's how I'm setting up the PWM:
void InitEPwm1(void)
void InitEPwm1(void)
{
//EPwm1Regs.
EPwm1Regs.TBPRD = 6000; // Set timer period
EPwm1Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Count up
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = 0; //TBCLK = SYSCLKOUT / (HSPCLKDIV × CLKDIV
EPwm1Regs.TBCTL.bit.PRDLD = 0;
EPwm1Regs.TBCTL.bit.PHSEN = 0;
// Setup compare
EPwm1Regs.CMPA.all = 3000;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = 1; // immediate mode
// Set actions
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // low on CMPA
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; //high on zero
}
I'm getting a pulse train but it's not working the way I want and I can't figure out why. I can't seem to influence either the frequency by changing EPwm1Regs.TBPRD nor can I influence the duty cycle by changing EPwm1Regs.CMPA.
All of the examples I've found are far more advanced then what I'm trying to do and in that sense, they aren't very helpful. There's just too much information in the peripheral guide and it's making my head spin. Any help would be greatly appreciated. Thanks.