Other Parts Discussed in Thread: CONTROLSUITE
I am looking for a a detailed application note on the sliding mode observer (s) for a PMSM controller. My motor is in reality a linear motor and I would like to use a sensorless technique to control it. It will run at the equivalent of 60,000 rpms, and I would like to use a 28335 to control it. The current loop is already more or less working, but I need to close the speed loop. In doing so, I am not sure if the SMO will do its job. I certainly need to operate at a much higer ISR and PWM frequency than both the PFC and Dual Motor control kits which I have bought and which I have been able to get going with CCS V4. I would like to get a better understanding of the SMO to see if I can rely on 28335 or if I must go to a different processor.
Thank you
Farouk