Part Number: TMS320F28379D
Hello,
I am working on TMS320f28379d and I would like to config Boot Mode pins. How could I change the GPIO72 and GPIO84 for another pair of pins?
For example, GPIO36 and GPIO38. As I want to use the GetMode/Flash, I have to set up both pins equal to "1".
From the spruhm8i I could see that it is possible change these pins using BOOTCTRL. However, I do not have any clue how I could change it in the firmware.
Moreover, I have a question:
Is it possible to Boot directly from the Flash (without any external pull-up)?
In the case that I do not have any free pin and I do not want to share any pin with the boot mode
Thanks for your helping,
Best Regards.