Hi, Experts,
I have a question about the CLB input/output pin settings like the following thread.
:https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/838650?TMS320F28379D-Pins-of-CLB
We understand that "Each CLB has multiple inputs and outputs which can be routed to I/O pins via the X-bars if desired."
So I have a question about the number of pins that can be set.
1)Is the maximum number of I/O pins that can be assigned as input to 1 CLB module 8 PINs?
2)Is the maximum number of I/O pins that can be assigned as output from 1 CLB module 16 PIN? (It duplicates, so it has the same signal, but ...)
Best regards,
O.H