Hi,
I need to reduce the clock frequency in order to reduce the power consumption, i need to keep CAN, SCI and ADC working under reduced
clock frequency.
at sprugl8b TMS320F2803x Piccolo System Control and and Interrupts Reference Guide (Rev. B) page 43 there is the note below:
The input clock and PLLCR[DIV] bits should be chosen in such a way that the output frequency of the PLL (VCOCLK) is a
minimum of 50 MHz.
so i understand that the minimum clock frequency at CPU can be 50MHZ / 4 = 12.5MHZ
that is right ?
thanks in advance