Other Parts Discussed in Thread: TMDSCNCD28388D
Dear TI expert,
We want to use the TMS320F28388D with two different configurations: one using both Ethercat links and the other using only one Ethernet link. Both configurations will have different firmware versions.
To save space and components in our board (is a very space coinstraint application), we are thinking about connecting the Ethernet lines to the same PHY module as Ethercat link1, effectively short-circuiting the ENET and ESC1 lines in our board. When working with Ethercat, the Ethernet peripheral would be disabled in the MCU and, when working with Ethernet, the Ethercat peripheral would be disabled in the MCU.
Do you see any inconvenient in short-circuiting the ESC1 and ENET signals and sharing the same PHY module? The PHY module we intend to use is DP83822HFRHBR. In which state do you recommend to configure the disabled pins?
Thank you very much for your answer.