Tool/software: Code Composer Studio
Hello
Please contact us for any problems while using DSP product TMS320F2808.
We have confirmed that there is no problem with the program source as a mass-produced product.
It is programmed to read one AD input value and do two actions on it.
One is set to operate corresponding to this value in hardware.
The other is to set the range of this value so that if it is out of the set value, a warning is sent by communication.
Is set.
However, the AD value is alerted temporarily by communication.
At this time, the input AD value is normal and the hardware set to operate with this value operates normally.
So, the actual hardware operates normally, but displays an error by communication.
This behavior is not a continuous phenomenon and occurs very occasionally.
question :
This part is thought to have been damaged by the memory programmed in the TMS320F2808 chip.
Why does this happen?
Thank you.