This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MOTORWARE: Teknic M-2310P-LN-04K

Part Number: MOTORWARE

Tool/software: Code Composer Studio

Hi, 

I ordered the Teknic M-2310P-LN-04K motor from TI website and I am working with the motorware labs meanwhile, should I mention my voltage power supply in the user.h

I am using 24V/5A. 

One more question, Its rated speed is 6000 rpm and of 7.1 Continues Curren, but at which voltage supply could I reach those values. What is the maximum speed this motor can reach with 24V supply? 

Thanks

  • That depends on the loading added on the motor. The power supply should be ok for the motor run with the maximum speed if the motor is not running with the heavy load. You might use a high output current power supply if possible, like 24V/36V,10A.