Part Number: TMS320F28030
Hello, several GPIO, are defined as outputs, when the power turn off the output glitchs, resulting in a change in down stream logic.
Can you suggest a firmware fix that would mitigated this issue..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28030
Hello, several GPIO, are defined as outputs, when the power turn off the output glitchs, resulting in a change in down stream logic.
Can you suggest a firmware fix that would mitigated this issue..
Per datasheet, GPIO19, GPIO34-38 do not have glitch-free I/Os. Not sure if these are the I/Os you are referring to. You have not attached a scope shot to depict exactly what you mean by "glitching" and how it affects components downstream.
Per datasheet, GPIO19, GPIO34-38 do not have glitch-free I/Os. Not sure if these are the I/Os you are referring to. You have not attached a scope shot to depict exactly what you mean by "glitching" and how it affects components downstream.
where is this found in the data sheet
would disabling the BOR help
Please see section 5.12 in page 32 of SPRS584M.
After reset, all GPIO pins are inputs. One option would be to reconfigure GPIOs to inputs before powering off. Please attach a scope shot that clearly shows the following signals during power-off: 1.8v, 3.3v, -XRS, a GPIO pin that exhibits the problem.
You may want to look into an external SVS chip, which would activate -XRS upon power-down. This would keep the GPIO pins in high Z.