Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Dear TI Hello,
I am using the Signal Generator library for C28x DSP,
I couldn't find a clean sinus wave using the SGENT_1 (look up table).
My interrupt is triggered every 50us (20Khz) as in the sgen_mdl pdf file.
C code:
typedef struct {
unsigned int freq;
unsigned int step_max;
unsigned int alpha;
int gain;
int offset;
int out;
void (*calc)(void *);
}SGENT_1;
#define SGENT_1_DEFAULTS { 5369,\
1000,\
0,\
0x7fff,\
0,\
0,\
(void (*)(void *))SGENT_1_calc}
SGENT_1 sgen = SGENT_1_DEFAULTS;
int32 t_i32SinusBuf[SINUS_BUF_LEN];
interrupt void
Timer0_ISR(void)
{
volatile static int32 s_i32Sinus;
static int32 *s_pi32SinusBufPtr = t_i32SinusBuf;
/* Acknowledge this interrupt to receive more interrupts from group 1 */
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
/* Clear Timer interrupt flag */
CpuTimer0Regs.TCR.bit.TIF = 0;
/* Increment the timer0 interrupt counter */
CpuTimer0.InterruptCount++;
/* Update sgen macro */
sgen.calc(&sgen);
s_i32Sinus = sgen.out;
/* Write sins to buffer */
*s_pi32SinusBufPtr++ = s_i32Sinus;
if( s_pi32SinusBufPtr == (t_i32SinusBuf + SINUS_BUF_LEN))
{
s_pi32SinusBufPtr = t_i32SinusBuf;
}
}
I am using a 50 int32 buffer to display out using Single time scope.
Thank you in advance,
S.Tarik,