This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Code Composer Studio™ forum

Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, BOOSTXL-3PHGANINV

Tool/software: Code Composer Studio

I'm trying to run the Level1 build from the SPRACO3 Application report, utilizing LAUNCHXL-F28379D and BOOSTXL-3PhGaNInv

The project  build done without errors. After debug, and run the project on the launchpad, i can see totally different values in the Expression view compared to the ones in the Application report.

For example 2989 instead of the expected 0 or 1 in the value field of enableFlag. Also @data instead of @program in the Address field of the Expressions view.

According to the Application report I should change enableFlag from 0 to 1, however it is not possible.

Practically it seems, every variable/expression has incorrect values. Thus the program does nor work as it should.

I followed every step of the Application report. What did i missed/made wrong?

How can I resolve the issue?

I use the latest version of CCS: Version: 10.0.0.00010 

Thank you,

Zsolt