This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: PIE vector fetch error cause

Part Number: TMS320F280049


The F28004x TRM sprui33c mentions a NMI source called PIEVECTERR (PIE vector error).  Page 457 gives the only description of this I can find:

PIE Vector Fetch Error NMI Flag
This bit indicates whether a mismatch was detected during an
interrupt vector fetch. It can be cleared by a system reset or by
writing to the corresponding bit in the NMIFLGCLR register.
Reset type: SYSRSn
0h (R/W) = No vector fetch error detected
1h (R/W) = Vector fetch error detected

But this doesn't really say what causes this error.  What exactly is a vector fetch error?

Regards,

David