This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK2808 ?

Other Parts Discussed in Thread: TMS320F2808, TMS320F2811, TMS320F2812

Dear all

I am a student at the university of kasetsart, Thailand. I interest on TMDSDOCK2808. I want to know that what is including in developtool.

1. Does it include F2808 controlCARD and docking station right?

2. Dose it has JTAG on board for flash program TMS320F2808 right?

3. Can XDS100 USB JTAG Emulator is flash program TMS320F2808,TMS320F2811,TMS320F2812 right?

Please advice me. Thank you.

 

Best Regards,

Nakorn Threesinghawong

  • Nakorn,

    The features of the experimenter's kit are listed on the product folder here: TMDSDOCK2808

    http://focus.ti.com/docs/toolsw/folders/print/tmdsdock2808.html

    Nakorn Threesinghawong said:
    1. Does it include F2808 controlCARD and docking station right?

    Yes, see below in blue:

    The new C2000 Experimenter Kits from Texas Instruments are ideal products for OEMs to use for initial device exploration and testing. The 2808 Experimenter Kit has a docking station with access to all controlCARD signals, breadboard areas and RS-232, JTAG connectors, and features on board USB JTAG emulation. Each kit contains a 2808 controlCARD. The controlCARD is a complete board level module that utilizes and industry-standard DIMM form factor to provide a low-profiles single-board controller solution. . Kit is complete with Code Composer Studio™ IDE v3.3 C28x™ Free 32K Byte Version. C2000 applications software with example code and full hardware details also available. No external JTAG emulator is required as the docking station has on board USB JTAG emulation.

    Features

    • TMS320F2808 MCU based controlCARD
    • Docking station with on board USB JTAG emulation
    • Code Composer Studio™ IDE v3.3, C28x™ Free 32K Byte Version
    • Applications software and example code also available for download

    Nakorn Threesinghawong said:
    2. Dose it has JTAG on board for flash program TMS320F2808 right?

    Yes, you can load code directly into RAM for debug or you can program the flash using the supplied Code Composer Studio and on-board JTAG.

    Nakorn Threesinghawong said:
    3. Can XDS100 USB JTAG Emulator is flash program TMS320F2808,TMS320F2811,TMS320F2812 right?

    I'm not sure if I understand the question.  If the question is can you use an external XDS100 then yes, you can.

    -Lori

  •  If i build my TMS320F2808 board.

    1. Can it use with TMDSEMU100U-14T - XDS100 USB JTAG Emulator?

    2. Can TMDSEMU100U-14T - XDS100 USB JTAG Emulator  use with TMDSCCS2000-1 - C2000 Code Composer Studio IDE v3.3? if answer is yes, what version of XDS100 can use? V1 Or V2

    you answer is helpful for me. Because i would like to buy a correct tool for my project. Thank you.

    Best regards,

    Nakorn Threesinghawong