Other Parts Discussed in Thread: OPA4277
Hi,
While doing temperature cycle test from +60 to -25 deg C, we observed variation in the voltage reading approx 15% to 20%. Please find below the test result attached. We are unable to find details or datasheet related to F28335 ADC performance over temperature variation & method to compensate this variation. Even we have used industrial grade parts in the analog section design, like Opamps (OPA4277) -40°C to +85°C, Resistor ±25ppm/°C etc.
If anyone has come across such a problem or knows a solution please reply..
Regards,Ashutosh