Part Number: TMS320F28030
Tool/software: Code Composer Studio
Hello, data is transmitted via RS232 Bit bang, using the while loop there are no issues, the data s transmitted correctly with or without the debugger.
When the while loop is commented out the data is garbage (fail), with and without the debuggert
#define UART_WAIT_ONE_BIT for (delay1 = 1; delay1 <43; delay1++) {asm(" NOP"); asm(" NOP"); asm(" NOP");asm(" NOP"); asm(" NOP"); asm(" NOP"); asm(" NOP"); asm(" NOP"); asm(" NOP"); asm(" NOP");}
Uint8 FwRevision[] = {"12345678- A"};
PASS:
while(1){
tx_FirmwareSerialNumber(FwRevision);
}
FAIL:
//while(1){
tx_FirmwareSerialNumber(FwRevision);
//}
Sub
void tx_FirmwareSerialNumber(Uint8 *ptrFwRevision
Uint8 delay1,byteCount,mask,bitIndex;
byteCount = 11;
mask = 0x01;
byteCount = 0;
for(byteCount = 0; byteCount < 11; byteCount++){
//Send start Bit
GpioDataRegs.GPACLEAR.bit.GPIO23 = 1;
UART_WAIT_ONE_BIT
//Transmit 8 bits, shift the data
for(bitIndex = 0; bitIndex <8; bitIndex++){
if(ptrFwRevision[byteCount] & mask){
GpioDataRegs.GPASET.bit.GPIO23 = 1;
}
else
{
GpioDataRegs.GPACLEAR.bit.GPIO23 = 1;
}
//LSB First,
mask <<= 1;
UART_WAIT_ONE_BIT
}
//Tx Stop bit
GpioDataRegs.GPASET.bit.GPIO23 = 1;
UART_WAIT_ONE_BIT
UART_WAIT_ONE_BIT
UART_WAIT_ONE_BIT
mask = 0x01;
}//End while