Part Number: TMS320F280049
Other Parts Discussed in Thread: AMC1035,
Tool/software: Code Composer Studio
I am using SDFM module in TMS320F280049 with AMC1035.
I would like to have synchronized measurement with PWM1 module which generates signal at 50kHz .
My problem is when I enable synchronization from PWM1 and a particular interrupt from SDFM occurs I get a wrong results. The interrupt is invoked in periodic way of 20us which is as expected. When I disable PWM synchronization I can get a correct result in ISR. The PWM1 is configured to generate SOC_A when time-base counter is equal to period. So it should be
My configuration is following:
SDFM1 Filter Settings : Only FILTER4 is enabled, SINC3, OSR 128, SD_CLK = 10MHz, @ data rate frequency = 78kHz, latency 38.4us
Initialization code: It is based on example code from C2000 ware.
void init_SDFM(void)
{
//pin config
GPIO_setDirectionMode(58, GPIO_DIR_MODE_IN);
GPIO_setMasterCore(58, GPIO_CORE_CPU1);
GPIO_setPadConfig(58, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(58, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(GPIO_58_SD_D4);
GPIO_setDirectionMode(59, GPIO_DIR_MODE_IN);
GPIO_setMasterCore(59, GPIO_CORE_CPU1);
GPIO_setPadConfig(59, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(59, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(GPIO_59_SD_C4);
//
// Configure Input Control Unit: Modulator Clock rate = Modulator data rate
//
SDFM_setupModulatorClock(SDFM1_BASE, SDFM_FILTER_4, SDFM_MODULATOR_CLK_OFF);
SDFM_configDataFilter(SDFM1_BASE, (SDFM_FILTER_4 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(128)), (SDFM_DATA_FORMAT_16_BIT | SDFM_FILTER_ENABLE | SDFM_SHIFT_VALUE(0x0006)));
//
// Enable Master filter bit: Unless this bit is set none of the filter
// modules can be enabled. All the filter modules are synchronized when
// master filter bit is enabled after individual filter modules are enabled.
//
SDFM_enableMasterFilter(SDFM1_BASE);
//
// Set the output data format
//
SDFM_setOutputDataFormat(SDFM1_BASE, SDFM_FILTER_4, SDFM_DATA_FORMAT_16_BIT);
//
// Disable PWM sync
//
//SDFM_disableExternalReset(SDFM1_BASE, SDFM_FILTER_4);
//
// PWM signals can synchronize SDFM1 filters. Enabling PWM sync for SDFM
// filters.
//
SDFM_enableExternalReset(SDFM1_BASE, SDFM_FILTER_4);
SDFM_setPWMSyncSource(SDFM1_BASE, SDFM_FILTER_4, SDFM_SYNC_PWM1_SOCA);
//
// Enable interrupts
//
// Following SDFM interrupts can be enabled / disabled using this function.
// Enable modulator clock failure
// Enable data filter acknowledge
//
SDFM_enableInterrupt(SDFM1_BASE, SDFM_FILTER_4, (SDFM_MODULATOR_FAILURE_INTERRUPT | SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT));
/*
SDFM_disableInterrupt(SDFM1_BASE, SDFM_FILTER_4,
(SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT |
SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT));
*/
//
// Enable master interrupt so that any of the filter interrupts can trigger
// by SDFM interrupt to CPU
//
SDFM_enableMasterInterrupt(SDFM1_BASE);
}
Thank you.