This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem to install Driver of Texas instruments XDS510 DSP Emulator - RENF28335 Board

I want to install the RENF28335 DSP card under windows 10-64 bits, I installed CCS3.3 recommended by the technical document correctly, but when I wanted to install the Texas instrument XDS510 DSP emulator, it does not work, and gives me the error :

Error connecting to the target:
Error 0x80000240/-2082
Fatal Error during: Initialization, OCS,
Device driver: Emulation Connection Loss Detected on Target CPU.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.


I/O Port = 240

Board Name: F28335 XDS510 Emulator_1
Cpu Name: CPU_1

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.

Thank you for helping me to overcome this problem.