Other Parts Discussed in Thread: CONTROLSUITE
I am using ControlSuite 1.7 today. I cannot seem to use teh update feature to go from 1.7 to 1.9. This is true if I use the update within controlsuite or use the start menu icon for update. It goes out searches and finds version 1.9, but when I try to install it give a file association error8664.2010 01 21 ControlSuite Error update to V1.9.doc
from the atttached doc you can see the error, but it says " this file does not have a program associated wwith it for performing this action. Create an association in the folder options control panel?"
I hit OK, and then controlsuite update says " some of the updates failed to install properly."
couple notes:
using windowsXP
proxy - tried with it auto and non-auto
tired with and without firewall