Part Number: TMS320F28069F
Hello,
I'm using the InstaSpin Lab3b for speed control of a PMSM. It works well for most of the cases. The speed control performance is very good even below 10% Rated Speed of the motor, but I have a problem when the speed reference is 0. Is you manually spin the motor axle (with no load) the motor start to spin with low speed and high torque (torque sign is oppostite to speed sign) and it doen't stop even if you remove this manually generated force I had expected some oscillation, but not this continuous movement. Is this normal performance in sensorless control? Probably I have some parameters wrong configured? Any clue?
Thank you in advance,
Borja.