Dear C2000 team,
Can you help me with some clarifications?
Overview:
The datasheet for theTMS320F28035 quote a minimal fall time of tf(SDA) = 11.4ns for the I2C interface. The EEPROM with which it should communicate with has a minimal fall time of below 10ns. on the prototype both devices are communicating with each other. While reviewing the project the mismatch of 2-3ns was discovered.
Question:
Can you help me understand if there is a technical reason for the 11.4ns and if it is safe to leave the design as it is, or if a RC is required to "slow down" the fall time?
I am looking forward for your feedback.
Best regards,
Nico