This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28032: very slow interrupt execution

Part Number: TMS320F28032

Hi,

I am using a TMS320F28032 for a multi stage Flyback design.
So far everything is working as purposed.

Controller is clocked by a 20Mhz XTAL. SYSCLOCK is (measured with GPIO18) 60MHz and LSPCLK ist 15MHz.
I already set up 3 phase shifted PWMs with 100 kHz each (Period register is 600 in Count-Up mode). I see on my scope that those PWMs work as purposed (100kHz each and 120° phase shift each)

ePWM1 generates a SOC Pulse as soon as its counter is zero. This riggers my high priority SOCs 0 ... 2 to sample ADCIN0A,ADCIN0B and ADCIN1A
SOC2 is configured to throw an interrupt. (the only one so far on my controller!)

EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 0;      // INT pulse generation occurs when ADC begins conversion -> early interrupt
AdcRegs.INTSEL1N2.bit.INT1E = 1;                 // Enable ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 1;         // continuous sampling for ADCINT1
AdcRegs.INTSEL1N2.bit.INT1SEL = 0x02;       // End of conversion of SOC2 will trigger ADCINT1

AdcRegs.INTSEL1N2.bit.INT2E = 1;                 // Enable ADCINT2
AdcRegs.INTSEL1N2.bit.INT2CONT = 1;         // continuous sampling for ADCINT2
AdcRegs.INTSEL1N2.bit.INT2SEL = 0x07;       // End of conversion of SOC7 will trigger ADCINT2

AdcRegs.SOCPRICTL.bit.SOCPRIORITY = 0x03; // SOC0-SOC2 are high priority, SOC3-SOC15 are in round robin mode
EDIS;

The interrupt is periodically thrown in the right mannor right after SOC2_EOC. But is see already with some stupid data shifts or even only while acknowledging the Interrupt servicing takes rediculous long times.

typedef struct  ADC_Sampledata  ADC_Sampledata;

/*******************************************************************************
* UNION         : ADC_Data
* DESCRIPTION   :
* Allows a int to be written directly in to a _iq variable.
*******************************************************************************/
union Sample_ARG
{
    _iq15            m_IQ15;
    unsigned int     m_Int;
};
/*******************************************************************************
* STRUCT        : ADC_Sampledata
* DESCRIPTION   :
* contains the high speed sampled adc values
*******************************************************************************/
struct ADC_Sampledata
{
    Sample_ARG    AC_Input;
    Sample_ARG    Rail_Feedback;
    Sample_ARG    VIN_RECT;
};

/* align sample data array */
#pragma DATA_ALIGN ( Sampledata , 8 );
ADC_Sampledata Sampledata;

// ISR called at end of conversion of high priority fast ADCs
__interrupt void ADC1_EOC(void)
{
    GpioDataRegs.GPASET.bit.GPIO10 = 1;                          // on + off takes 260ns

    Sampledata.AC_Input.m_Int      =(AdcResult.ADCRESULT0)<<3;   //   takes about 580 ns
    Sampledata.Rail_Feedback.m_Int =(AdcResult.ADCRESULT1)<<3;   //   takes about 580 ns
    Sampledata.VIN_RECT.m_Int      =(AdcResult.ADCRESULT2)<<3;   //   takes about 580 ns

    //GpioDataRegs.GPACLEAR.bit.GPIO10 = 1;

    AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;       // Clear ADCINT1 flag reinitialize for next SOC  -  takes 540 ns
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;     // Acknowledge interrupt to PIE                  -  takes 240 ns
    GpioDataRegs.GPACLEAR.bit.GPIO10 = 1;
    return;
}

My programm is running from Flash.

remark: This is not my first project with this processor.
I already set up a multi kW active PFC. There i collect ADC data from 2 ADCs, calculate 32Bit Type-2 controlers (in assembler) and set new PWM values in an EOC Interrupt within 2µs. So i think i probably missed something somewhere, maybe you can give me a hint in the right direction.

Thank you!