Other Parts Discussed in Thread: MAX232
Tool/software: Code Composer Studio
Hi,
I am working on a project where I establish SPI communication between 2 TMS320F28379D Delfino Boards. I want to use the maximum speed which is 40 Mbps, with wires of length 100 cm; but when I used wires with length of 50 cm, and configured the SPI to run at speed higher than 6 Mbps the received data at the 2 sides of communication become corrupted, even at speed 6 Mbps when my hands touches the wires, the data become corrupted.
So, Is there any wires specification or electrical circuit to act as an interface between the MCU and the wires to overcome this signals interference?