This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: ADC input >12-bit and SPI 20MHz

Part Number: LAUNCHXL-F28379D

Hi all,

I need a DSP Board that has >12 bit resolution of ADC input and SPI with clock 20MHz.  I must to verify the performance of external 12-bit DAC, with FSO 5V and output analog signal every 17 clock edge. The reading rate of analog signal is 625kHz. I am thinking of trying to use a LAUNCHXL-F28379D, is this board adapt for this test?

Thank you and best regards

Francesco Buonomo