Part Number: TMS320F2808
Tool/software: Code Composer Studio
Hi TI E2E forum: Sometime ago I had purchased the C2000 ACDC Developer Kit . The TI part # for this kit is : TMDSACDCKIT. The ACDC EVM features are : 12VAC IN with 80W at 10A Output. The topology is 2 phase interleaved PFC + Phase shifted full bridge. This EVM uses the F2808 control card which is a plug in card that has edge card connector. I have lost the C2000 Application software that came with this and the example code. Also I will need the documents that has the schematic etc. Can you please help by sharing the software package with example code that came with this EVM?