Hello
I am integrating one of my Applications with Flash API.
The combined code got compiled properly and even I started debugging the code.
The Flash API part is working fine i.e. reading/ writing both is working good.
But when I call user defined functions for initializations, the debugger stops ending up with the message as:
"Break at address "0x3ff7eb" with no debug information available, or outside of program code"
I am not getting the exact issue, should I need to modify the linker file?
I request you to go through the same and please guide me further.
Thanks and Regards,